Stäubli is a global mechatronics solution provider with four dedicated Divisions: Electrical Connectors, Fluid Connectors, Robotics and Textile. We are an international group that currently operates in 28 countries.
The reliable inspection, labelling and packaging of 36,000 syringes per hour places high demands on automation. Stäubli robots master this task under hygienic conditions.
Competitive pressures are always driving new concepts in manufacturing. The Czech supplier ACL Automotive has entrusted the machining of roof rails to Stäubli robots and is very satisfied with the results.
The weaving mill “Tessitura Nesi Fausto & Nesi Silvano” is a company with over 40 years of know-how in weaving process using the Stäubli SAFIR as their main solution.
Czech manufacturer Kiekert produces around 180,000 motor vehicle locks per day. An intelligent robotic cell for in-line X-ray inspection, featuring a Stäubli TX60 six-axis robot, ensures the highest quality standards.
Control units for automotive safety systems must function perfectly under all conditions. One-hundred percent testing is mandatory. Thanks to robotics, ...
Four Stäubli SCARAs prove their worth in the production of oil level sensors. These highly dynamic four-axis machines pick up punched parts and connectors, ...
While the development of composite exterior parts for vehicles takes place on computer systems, production is still dominated by manual labor. An Austrian manufacturer has made the switch to robot ...
Stäubli robots play a central role in the production of vaccines. The large six-axis TX200 Stericlean robots are used to shake and tilt so-called “cell factories” ...
Control units for automotive safety systems must function perfectly under all conditions. One-hundred percent testing is mandatory. Thanks to robotics, ...
Three Stäubli robots in a fully automated system implemented by system integrator KUM Technic on behalf of Belgian pharmaceutical company Diagenode work toward one goal: the reliable ...
The fully automated process takes cell culture processing from the lab to the mass production line. The key is the Stäubli TX60 Cleanroom robot which is equipped to ...
Reliable contact technology for the world's largets network of high-speed trains: Stäubli supplies high-power connectors for traction converters that find use in the newest generation of trains.
For their individual, mobile transport platforms, the specialist from the Nuremberg region relies on robust Stäubli connectors to transmit the power in its electric drive systems.
Thanks to Stäubli QMC 122 magnetic clamping solutions, we've been able to increase our production level, improve workshop responsiveness, reduce occupational health risks ...
A new Jacquard installation with the large-format Stäubli LXL Jacquard machine and an end-to-end harness at TextielMuseum offers new creative weaving possibilities to artists and designers.
Stäubli robots play a central role in the production of vaccines. The large six-axis TX200 Stericlean robots are used to shake and tilt so-called “cell factories” (culture chambers) ...
A pioneering project: Installing a solar system in the Antarctic. For reliable connection and safe power transmission, the Artigas base relies on high-quality PV connectors from Stäubli.
Stäubli robots play a central role in the production of vaccines. The large six-axis TX200 Stericlean robots are used to shake and tilt so-called “cell factories” ...
Automotive manufacturers are demanding greater precision from anti-lock braking systems. These exacting specifications can no longer be met with manual assembly lines...
Chinese manufacturer Yutong Bus churns out over 340 units a day and relies on Stäubli RX160L robots for its laser cutting operations. This top-mounted 6-axis robot delivers efficiency, speed and precision.
Currently, all plastic headlamp lenses come with a protective coating. Thanks to the latest generation of robots, transparent micrometer-thin protective layers can be accurately applied under cleanroom conditions.