Harsh environment for connection solutions in Swiss Alps
RAILWAY SUCCESS STORY

A close cooperation to withstand harsh environments

The Swiss Rhaetian Railway (RhB) transports thousands of people through the beautiful Swiss Alps, where climate conditions can be quite rough. To ensure comfort and security for the passengers, signals and data are sent through the complete train.

The business needs

RhB needed a new and highly stable system of electrical connectors between the train compositions to ensure that it signals can flow reliably during the train rides. Surroundings in the Swiss Alps can be harsh with possible temperature variations of up to 60° Celsius in a single ride. The new connection system has to feature 32 signal contacts and one data bus connector.

The challenge

The customer wanted to replace three outdated systems with only one that was state-of-the-art and would work in very tight space conditions. The solution needed to be resistant to high temperature variations, vibrations and mechanical shocks, but also mud, break dust, wet with dew and salt spray. At that project phase, RhB had already decided on one particular connector - however, not being fully sufficient. There- fore, the new system had to fit on this existing connection plate on the composition and was required to also resist hammer strokes in the event of icing.

The solution

In close cooperation with RhB Stäubli Electrical Connectors helped to set up the technical specifications and then developed a completely new solution. The housing is very robust and provides a handle for easy opening. A sufficient overlap of the contact parts will ensure that even under severe vibration and temperature fluctuations the contact is never interrupted. With a 15° departure angle of the plug to the vertical, mechanical stress of the cable is significantly reduced and the connector operation is extremely simplified. The construction of the cover lid prevents an accumulation of snow on the inside of the protective cover. The insertion of the connector is supported by two longitudinal pins, which means that the connector cannot tilt.

The added-value provided

Based on the broad experience in railway technology there was a common understanding between RhB and Stäubli Electrical Connectors on how to approach the design of the new connection solution. The innovative product solution exceeded the customer expectations and even includes features that the customer had not thought of.

The robust handle simplifies the operations and accelerates the composing of the wagons. The custom specific design and development integrating an existing connector saved conversion costs substantially. The special design with the two longitudinal pins prevents that pins are bent or knocked back and thus makes the connection very reliable and durable.

Stäubli Electrical Connectors faced the challenges very flexibly and cooperatively. Due to the unique features of this solution also other Swiss railway operators rely on it.

 “The customized solutions developed for our application have been subjected to detailed testing by Stäubli Electrical Connectors, so that we can guarantee our customers maximum operational reliability.” 

Confirms Leo Fäh, Rolling Stock Division, Head of Electrical Engineering at Swiss Rhaetian Railway (RhB)

APPLICATION

Market Segment: Railway

Industrial Connectors: tailor-made

Application: connector for harsh environment transmitting data and signals between the wagons
 

  • Easy and safe operation
  • Compact and space saving
  • Integrating an existing connector platform
  • Shock, vibration and pollution resistance

BENEFIT

  • Saving of conversion costs by tailor made solution
  • Optimized operational costs through reliable and durable connection in harsh environment
  • Timesaving coupling process of wagons due to innovative connector design
Inter-car coupling with multi-pole rail connector

Connection to transfer data, signal and power between the wagons

Customer conversation at RhB

Cooperative development of tailor-made connection solution

Coupling the connector at RhB

The robust handle simplifies the operations

The customized multi-pole connector at RhB

Two longitudinal pins prevent that pins are bent or knocked back

Icy and harsh environment in the Swiss alps

The connector solution withstands snow and ice